LTE FDD
For Real-Time capability.
This topic describes the settings of the Cell Parameters node.
Total Number of Resource Blocks
Total Number of Occupied Subcarriers
Number of Subcarriers for Resource Block
Number of Symbols for Resource Block
nDMRS-CSH-Identity (N_csh_DMRS_ID)
This setting specifies Cell ID.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:CIDentity <integer> [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:CIDentity? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:CID 20 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:CID? |
|
State Saved |
Yes |
|
Preset |
0 |
|
Min |
0 |
|
Max |
503 |
|
Initial S/W Revision |
A.14.00 |
Sets the antenna to be used for transmitting the uplink signal.
When multiple antennas are configured or the Fading contained in Waveform is set to On or the Number of HARQ Processes is not set to 8, it's hidden.
See 3GPP TS 36.211 for more information.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:APORt <integer> [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:APORt? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:APOR 2 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:APOR? |
|
Dependencies |
Selectable values depend on Total Number of Antennas. |
|
State Saved |
Yes |
|
Preset |
0 |
|
Min |
0 |
|
Max |
0 (1 Antenna) 1 (2 Antennas) 3 (4 Antennas) |
|
Initial S/W Revision |
A.14.00 |
Sets the total number of physical antenna port configuration used for uplink transmission in this cell. See 3GPP TS 36.211 for more information.
In the case that Number of HARQ Processes is 3 or 4 (TTI Bundling is on), Total Number of Antennas is set to '1 Antenna' as read-only.
When multiple antennas are configured, this setting is read-only.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:APORts:COUNt <integer> [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:APORts:COUNt? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:APOR:COUN 2 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:APOR:COUN? |
|
Notes |
Valid values: SCPI: 1 | 2 | 4 GUI: 1 Antenna | 2 Antennas | 4 Antennas |
|
State Saved |
Yes |
|
Preset |
1 |
|
Min |
1 |
|
Max |
4 |
|
Initial S/W Revision |
A.14.00 |
This setting specifies the system bandwidth and number of Resource Blocks (RB).
When the system bandwidth is changed, the software automatically adjusts the value in the Total number of Resource Blocks cell, the Total number of Occupied Subcarriers cell and so on.
Note: The resource blocks and some parameters are reconfigured by changing the System Bandwidth parameter.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:BANDwidth|BWIDth B1M4|B3M|B5M|B10M|B15M|B20M [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:BANDwidth|BWIDth? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:BAND B10M :RAD:LTEF:WAV:RTIM:CCAR:ULIN:BAND? |
|
Notes |
BWIDth SCPI node is an alias of BANDwidth. |
|
State Saved |
Yes |
|
Preset |
B10M |
|
Range |
1.4 MHz (6RB)|3 MHz (15RB)|5 MHz (25RB)|10 MHz (50RB)|15 MHz (75RB)|20 MHz (100RB) |
|
Initial S/W Revision |
A.14.00 |
Display the number of resource blocks.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:RB:COUNt? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:RB:COUN? |
|
Notes |
Query only |
|
Dependencies |
The value in this cell is set by the software based on the System Bandwidth setting. |
|
State Saved |
No |
|
Preset |
50 |
|
Min |
6 |
|
Max |
100 |
|
Initial S/W Revision |
A.14.00 |
Display the total number of occupied subcarriers.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:SCARrier:COUNt? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:SCAR:COUN? |
|
Notes |
Query only |
|
Dependencies |
The value in this cell is set by the software based on the System Bandwidth setting. |
|
State Saved |
No |
|
Preset |
600 |
|
Min |
72 |
|
Range |
1200 |
|
Initial S/W Revision |
A.14.00 |
Displays the subcarrier spacing for the uplink. Only the 15 kHz subcarrier spacing is supported in this release.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:SCARrier:SPACing? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:SCAR:SPAC? |
|
Notes |
Query only |
|
State Saved |
No |
|
Preset |
F15K |
|
Range |
Value SCPI 15 kHz F15K |
|
Initial S/W Revision |
A.14.00 |
Sets the cyclic prefix, select a Normal or Extended cyclic prefix. The software sets Number of Symbols for Resource Block based on the cyclic prefix selection.
Cyclic Prefix is automatically set to Normal when Resource Allocation Type 3 is changed to on.
Resource Allocation Type 3 is automatically set to off when Cyclic Prefix is changed to Extended.
See 3GPP TS36.211 5.2.4 for more information.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:CP NORMal|EXTended [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:CP? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:CP NORM :RAD:LTEF:WAV:RTIM:CCAR:ULIN:CP? |
|
State Saved |
Yes |
|
Preset |
NORMal |
|
Range |
Normal | Extended |
|
Initial S/W Revision |
A.14.00 |
Displays the number of consecutive subcarriers in an uplink resource block.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:RB:SCARrier:COUNt? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:RB:SCAR:COUNt? |
|
Notes |
Query only, Fixed value |
|
State Saved |
No |
|
Preset |
12 |
|
Min |
12 |
|
Max |
12 |
|
Initial S/W Revision |
A.14.00 |
Displays the number of consecutive OFDM symbols in an uplink slot.
The software sets Number of Symbols for Resource Block based on the Cyclic Prefix selection.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:RB:SYMBol:COUNt? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:RB:SYMB:COUN? |
|
Notes |
Query only |
|
Dependencies |
Cyclic Prefix |
|
State Saved |
No |
|
Preset |
7 |
|
Min |
6 |
|
Max |
7 |
|
Range |
7 (for Normal Cyclic Prefix), 6 (for Extended Cyclic Prefix) |
|
Initial S/W Revision |
A.14.00 |
Sets the state of PUSCH DFT Swap.
PUSCH DFT Swap influences how data is mapped to resource elements in the physical uplink shared channel after discrete Fourier transform is performed. PUSCH DFT Swap can be turned on or off to provide two different interpretations of how data should be mapped to resource elements in PUSCH channels.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:PUSCh:DFTSwap[:STATe] OFF|ON|0|1 [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:PUSCh:DFTSwap[:STATe]? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:PUSC:DFTS 1 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:PUSC:DFTS? |
|
State Saved |
Yes |
|
Preset |
OFF |
|
Initial S/W Revision |
A.14.00 |
Set one or both of the following parameters to On to allow manual control of Hopping:
PUSCH Auto-calculate per-slot params
PUCCH Auto-calculate per-slot params
Sets Group Hopping or Sequence Hopping or to turn hopping Off.
See 3GPP TS36.211 for more information about Group Hopping and Sequence Hopping.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:HOPPing OFF|GROup|SEQuence [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:HOPPing? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:HOPP GRO :RAD:LTEF:WAV:RTIM:CCAR:ULIN:HOPP? |
|
State Saved |
Yes |
|
Preset |
OFF |
|
Range |
Off | Group Hopping | Sequence Hopping |
|
Initial S/W Revision |
A.14.00 |
Sets the state of nDMRS-CSH-Identity to enabled or not.
See 3GPP TS36.211 5.5.2.1.1 for more information.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:NDMRs:CSH:ID:STATe OFF|ON|0|1 [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:NDMRs:CSH:ID:STATe? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:NDMR:CSH:ID:STAT 0 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:NDMR:CSH:ID:STAT? |
|
State Saved |
Yes |
|
Preset |
OFF |
|
Initial S/W Revision |
A.14.00 |
Sets a value of nDMRS-CSH-Identity (N_csh_DMRS_ID).
This parameter is active only when nDMRS-CSH-Identity Enable is on.
See 3GPP TS36.211 5.5.2.1.1 for more information.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:NDMRs:CSH:ID <integer> [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:NDMRs:CSH:ID? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:NDMR:CSH:ID 1 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:NDMR:CSH:ID? |
|
State Saved |
Yes |
|
Preset |
0 |
|
Min |
0 |
|
Max |
509 |
|
Initial S/W Revision |
A.14.00 |
Sets nDMRS(1) value which is given by 36.211 Table 5.5.2.1.1-2.
This value is used for both PUSCH and PUCCH.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:NDMRs:ONE <integer> [:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:NDMRs:ONE? |
|
SCPI Example |
:RAD:LTEF:WAV:RTIM:CCAR:ULIN:NDMR:ONE 8 :RAD:LTEF:WAV:RTIM:CCAR:ULIN:NDMR:ONE? |
|
Notes |
Valid values: 0, 2, 3, 4, 6, 8, 9, 10 |
|
State Saved |
Yes |
|
Preset |
0 |
|
Min |
0 |
|
Max |
10 |
|
Initial S/W Revision |
A.14.00 |